Hi,
I tried to connect the tablet to the J28 input or the J29 input to charge it.
When there is a power connection at input J30 (USB-C from charger) via charger there is no charging of the tablet, and when the power connection at input J31 (DC Barrel Jack) then only at high voltages (above 10V) the tablet starts to charge.
Is it possible to charge the tablet only with a 5 volt input?
Thanks
Dvir