This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848J: About LED Behavior issue

Part Number: DP83848J

Hi Sir 

We used DP83848J for development and below is the schematic 

we found the behavior of LED_Speed is different. 

1. after system power-on without connecting cable, the LED_Speed is on.

2.after finishing system bootup, the LED_Speed is off. we measured this pin is High(3.3V)

Based on the spec's description, LED_Speed is off. -> the PHY's status is 10Mb/s

Q1. we measured RX_CLK and TX_CLK, they are 25Mhz. Based on spec's definition, it should be 100Mb/s in 25MHz of TX_CLK/RX_CLK ?

Q2 we had some boards below above procedures, but  LED_Speed is on.  we measured this pin is 1.375V(low) 

below is the register comparison table. the difference is register 0x10

LED_ON

LED_OFF

Please advise

BR

Yimin