This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83620: BMSR_ANEGCAPABLE is set to 1 even when configured on fibre mode

Part Number: DP83620

BMSR register value is 111100011001101 even when using FX mode, which doesn't allow auto negotiation. Note however that bit 3, AUTO-NEGOTIATION ABILITY appears a 1, so typical drivers aren't able to use this information to disable autonegotiation.

I'm thinking of using alternatively bit 12 of BMCR, AUTO-NEGOTIATION ENABLE to check strap initial value al rest, but this doesn't seem like the proper way to do it. Any suggestions?

Thanks!