This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Qualcomm Quick Charge selection IC

Prodigy 20 points

Replies: 3

Views: 112

Hello,

i'm looking for a IC which is located on the "Client" (like a Phone, Tablet, ...) side of a USB QC wall adapter.

Does something like a USB-C Interface (Power Management) IC exist, which:

 - can select the VBUS voltage via Quick Charge 2, 3 and 4 Interface (continuous mode)

 - has a Microcontroller Interface like SPI or I2C

 - optional: can monitor the VBUS voltage and or current

 - optional: has a fixed 3.3V output for the Microcontroller

  • Hello Wolfgang,

      I'm confused by your reference to Qualcomm.  Are you wanting to interface to a Qualcomm IC, if so, which one?  A block diagram would be helpful.

    Regards,

    ~Leonard

  • In reply to LeonardEllis:

    Hi Leonard,

    i gave it a try and drew a diagram:

    On the left side is a random USB Quick Charge wall Adapter. On the right side is my Device.

    The Charger Interface IC on the "existing USB charger" side, would be a Qualcomm Quick Charge compatible IC (which IC doesn't matter, as long as it uses the Qualcomm QC standard).

    And on my circuit is the IC I'm looking for. This IC is talking to the Charge Interface IC via D+ and D- to control the VBUS Voltage.

  • In reply to Wolfgang Gerdenitsch:

    Hi Wolfgang,

    Unfortunately, we do not have a USB Type-C Controller that supports Quick Charge. Our Type-C PD controllers are compliant to the USB PD standard and can provide higher power and current through USB Power Delivery.

    Thank you,
    Eric

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.