DS90UB940-Q1: MIPI short packets and CSI Virtual Channel identifier

Prodigy 10 points

Replies: 1

Views: 74

Part Number: DS90UB940-Q1

Greetings,

Does the DS90UB940 send the MIPI short packets (e.g. frame start, frame end) on the same virtual channel as programmed in CSI_VC_ID, or are they fixed to MIPI virtual channel 0? I have a case where image capture only seems to receive the synchronization information when using virtual channel 0. Thank you.

Best Regards,

Craig

1 Reply

  • Hello Craig,

    We will check into this early next week and respond back to see if we see the same issue. 

    Best Regards,

    Casey