This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO721M truth table

Expert 2435 points

Replies: 1

Views: 1835

Regarding ISO721M:

 

1)     When Vcc1(pin1) is 3.3V, Vi (pin2) is high Z, Vcc2(pin 8) power is off (low impedance),  is there any problem running part like this long term?

 

2)     What is the output level Vo (pin 6) when Vcc1(pin1) is off, Vi (pin2) is high Z, Vcc2(pin 8) power is on.

3)    Is there any problem running part like this (see question 2)?

Regards,

-Tim Starr on behalf of BS

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.