This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO721 isolation voltage

Intellectual 460 points

Replies: 1

Views: 323

I have an application that requires up to 1200V between the input side of an isolator and the output side.  I see from the specifications in the ISO721 datasheet that it lists a working "insulation" of 560V-peak.  Does this mean that I should not use this isolator?  Are there other isolators that are at least 100Mbps that could meet my 1200V requirement?

Thank you

  • Yes, you should not use ISO721 if your application requires 1200Vpk continuous operating voltage between input and output sides.

    We don't have a single channel isolator with 1200Vpk working voltage but we have 2, 3, and 4 channel isolators that meet this requirement. You can consider ISO7521C, ISO7631FC or ISO7641FC for your application.

    Saleem Marwat

    System Engineer

    Isolation Products, Texas Instruments

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.