This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 2035
Dear Sir/Madam/Miss,
Do HD3SS6126 chip support for 8:1 multiplexer (USB 3.0)? Since its only designed for 2:1/1:2, I'm wondering can I cascade it into 8:1.
Is that will be a problem in signal integrity if I cascaded it into 8:1 using this chips ? I had attached a picture file for better view.
Hello,
I think that it can be done, please give me more time to confirm whether is possible or not.
Regards
In reply to Elias Villegas M.:
Dear bro,
Hereby I had attached a picture of another new idea for 8:1 mux using HD3SS6126
Based on the new idea, can I connect all the HSA +/- pin, SSA0 +/- pin and SSA1 +/- pin together respectively ?
Is that any user had implemented it ?
How about the signal integrity ?
I had drawn and uploaded it "BlockDiagram3.png".
Kindly waiting for your reply bro.
Thanks
Regards,
Shagilan Bala
Dear Sir/Madam/Sis/Miss,
Hereby, I had attach a new picture of 4:1 multiplexer for USB 3.0.
Is this diagram ok for me to develop this project ?
How about its transmission delay & signal integrity?
\
In reply to Shagilan Bala:
Sorry for the delay.
I recommend you to use a USB hub instead. With your current implementation only one USB device will be available and every time you switch to another device it will have to be re-enumerated.
All the devices will be available at any time if you use a USB hub.
I recommend you to look at the TUSB8041, TUSB8020B.