I have a board that uses the TSB41AB2 to provide two IEEE-1394a ports. This is a research "product" that is used at many different Universities. There have been several failures in the field, where one of the two ports stops working. The failures have the same characteristics as the "late Vg event" failures reported in SLEA072A.
My nodes are self-powered, however. I am using the 6-pin connectors, but do not use Vp on the board (i.e., Vp is only connected to the two connectors). The design files (Altium format) are here: https://github.com/jhu-cisst/mechatronics-boards/tree/master/FPGA1394. There is also a PDF of the schematics.
I do not have the TPx diodes recommended in SLEA072A, but my connector shells are grounded. As far as I can tell, the only possible failure (in my case) might be if Vp somehow gets on one of the TPx lines. Is this possible? Are the protection diodes recommended even for a self-powered node?