I use Multiprotocol R232/RS422 Transciever. Transciver has RS232_TX, RS232_RX, RS422_TX_P, RS422_TX_N, RS422_RX_P and RS422_RX_N. I want to protect these signal against ESD to using only single ESD Protection Chip. TI advise TPD2E007 for RS232/RS485/RS422. TPD2E007 protect only two signal. I have to use three TPD2E007 with my single multiprotocol Transciever to esd protection. Also I am using 12 multiprotocol transciever on PCB Board. So I have to use 36 TPD2E007. I didtn't see RS232/422/485 expression in application area of multichannel ESD protection product datasheets.
Could you advise me multichannel ESD Protection chip like TPD2E007 structural design(bidirectional TVS etc.)?
Can I use TPD4E02B04, TPD4E6B06 and TPD4E101 products for RS232/422 ESD protection?