This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 537
Hello,I have a question about LMH0034 and LMH0031.
The investigating system is as follows.
<The camera output> - HD-SDI - 1920×1080 59i/50i/30p/29.97p/25p
<The CPU input : i.MX6> - Parallel interface - SMPTE274(1080i/p) SMPTE296(720p) - I/O : 1.8V
Can I realize the system by using LMH0034 and LMH0031?
Regards,Dice-K
Greetings,
Please note LMH0031 does not support 59.9i and 29.97p video frame format. Otherwise, using LMH0034 and LMH0031 can support this application.
Regards,,nasser
In reply to Nasser Mohammadi:
Hello nasser,Thank you for your reply.
Do you have a device supporting 59.9i and 29.97p video frame format?
Best regards,Dice-K
In reply to Dice-K:
Hello,
Please take a look at LMH0340/LMH0341 FPGA IP. Here is a link to this solution and documentation:
http://www.ti.com/tool/broadcast_video_serdes_ip
Please note: This IP supports 3G SDI video frame formats(on top of HD and SD video frames).