This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP mode(Short frame sync), Fs(min)=8kHz / PWM Modulator , I2C input Audio amp

Guru 20090 points

Other Parts Discussed in Thread: TAS5558

Hello,

Are there any device which can be used for the following specification?

- Linear PCM
- 16 bit
- Slave Mode
- SCLK=2.048MHz
- Fs=8kHz
- MSB First
- Short Frame sync(DSP mode)

Best Regards,
Ryuji Asaka

  • Hi, Asaka-san,

    Can you please provide more information about the system application so we can find the best solution for you?, like output power, processing options, etc. I would like to recommend you to take a look to our Audio Selection Tool as it is a good starting point to find the right device for your application.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • Hello Diego san,

    The customer request the PWM modulator device but I couldn't find the device which include the following specification.
    I will check the more detail to the customer but I would like to know all of the device witch can be used for these specification.
    Then I will promote the device to the customer.

    - Fs=8kHz
    - Short Frame sync(DSP mode)

    Best Regards,
    Ryuji Asaka
  • Hello Diego san,

    Please see the following as the requirement.

    -Mono Speaker
    -Output Power 20W(16ohm)
    -There is no Dynamic range , THD specification requirement.

    Best Regards,
    Ryuji Asaka
  • Hi, Asaka-san,


    Thanks for the information. I am not sure if we have a device compliant with the specs you mention, so, I have asked my colleague that supports PWM modulators to check your question. As he is traveling now, he may be able to get back to you in the next couple of days. 

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • Hello Diego san,

    Thank you for the checking.
    I'm looking forward to your reply.

    Best Regards,
    Ryuji Asaka
  • Hello Ryuji,

    Our most flexible DSP PWM modulator is the TAS5558. I would suggest reviewing the datasheet material to see if it meets your specs.

    Best Regards,
    Matt