Hi Team,
The customer is using TL16C554A for the 80pin device.
The issue is the local bus of TL16C554A can not communicate with XuPCI954. The local bus are the LBRST, nLBCS0~nLBCS3 ,nLBWR nLBRD ,LBA0~LBA2 and LBD0~LBD7 in the customer's schematic. Look the attachment, it is the schematic.
Q1: Is the schematic correct? If it is correct, is there any reason for the issue?
Q2: The customer wants a reference schematic for TL16C554A. Can you send me the reference schematic for TL16C554A?
Thanks,
Best Regards,