Hi Team,
I see similar posts, however, please allow me to post to clarify the TCA9517 requirement.
Below are the datasheet descriptions. Here, I have two questions.
Without the maximum value of VIL(B-side), customer would not be able to design system which operation is guaranteed.
[Q1]
What is the maximum VILC accepted for TCA9517 to avoid bus contention ?
We need to clarify what is the guaranteed voltage so that customer system would not have any problem.
If VILC=0.4V is the MAX instead of TYP, please let us know.
However, VOL_MIN - (VOL-VILC_TYP) is 0.38V. Regarding this spec, I was thinking that required VILC may be lower than 0.4V.
[Q2]
Why is "VOL-VILC" spec stated for ? It is also confusing that calculation result is not matching. (0.52 - 0.070 != 0.40)
I believe it is described to let user know the lowest voltage what TCA9517 can operate without any problem.
However, we need the worst condition information.
Best Regards,
Kawai