This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125BR800: SMB Equalization Range

Prodigy 140 points

Replies: 3

Views: 314

Part Number: DS125BR800

Hi,  We are using this part as a probe on a PCIe Gen3 link. Do you have a more detailed listing of the 256 different equalization settings? We would like to explore whatever total gain is available, but with less HF boost. In other words, set it up to be as flat as possible gain over the frequency range. Does it use an AGC loop to achieve the VOD settings?

Thank you,

Austin

3 Replies

  • Hi Austin,

    To achieve a flat gain curve, I would switch over to the DS125BR820 and use the minimum CTLE setting.

    This will produce the flattest possible curve.  The DS125BR800 has a multi-stage CTLE which will result in higher gain settings even with the lowest settings.

    Regards,

    Lee

  • In reply to Lee Sledjeski:

    Hi Lee,

    We would like more gain than 10dB. Do you have the settings for the DS125BR800 ?
  • In reply to austin mack:

    Here are the equalization values for all the pin configurations.  These give a very good spread from minimum to maximum CTLE.

    Regards,

    Lee

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.