Other Parts Discussed in Thread: DS92LV2411
Hello,
I have a DS92LV2411 and a DS92LV2412 on one PCB that are functioning properly in BIST mode and with static signals at the input of the 2411.
When applying a signal of about 10kHz the 2412 loses the PLL-LOCK state.
The clock frequency of the 2411 is 5MHz, all strap pins are 0, startup delay of VDD and PDB is 200ms for correct configuration detection.
All supply voltages are blocked, the measured ripple is round about 5mV.
Thanks
Mario