Other Parts Discussed in Thread: TUSB321
Dear Community
For a project we use a USB-PD adapter with our device in Upstream Facing Port (UFP) mode. So our device is a normal consumer of the USB power (e.g. 5V, 3A)
To get any energy out of a USB-PD adapter, a "hand shaking" on the CC pins of the USB type C port is needed. I discovered the TUSB321AI as a nice standalone solution, to get 5V and 3A from a USB-PD port. From several documentations I figured out, that the same result can be achieved with a pull down of the CC lines by two 5.1kOhm resistors to GND.
Can someone tells me, why there is the TUSB321AI chip for UFP mode, if the same can be achieved with two resistors? Am I wrong?
Thank you for your support.
Felix