The datasheet recommends the following configuration at the input to the DS30EA101:
If instead at the input the ac caps and the terminating resistor locations are reversed as shown below, what would the implication be? Would the DS30EA101 operate as behaved? Why does the ac cap need to be located closest to the input of the device instead of the terminating resistor? Is there a difference electrically?
Thanks,
Mark Heh