This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2513A-Q1: Voltage specification of D±

Part Number: TPS2513A-Q1

Hi,

I got following question from my customer.

They would like to know  voltage specification of D± which USB device can recognize each modes of charger for their reference.

Could you fill blank of attached file?

 Voltage specification.xlsx

They confirm if TI's port controllers are satisfied with them.

Best Regards,

Kuramochi

  • Hi TQ,

    I believe the min and max for the Divider 3 and 1.2V mode are on the EC table of the datasheet (look below):

    For the BC1.2 (CDP) voltages, please refer to section 8.3.1 (page 9 of DS) on the voltage levels. Thank you for using our parts. I hope this helps :-)