Other Parts Discussed in Thread: TIC12400-Q1
I am trying to configure the device in sleep mode so that any switch state change it gives interrupt to MCU
and for interrupt mode, the trigger is required or not. what is the proccess for it
DEVICE_ID = 0x01000000;
INT_START = 0x02000000;
CRC = 0x0300FFFF;
IN_STAT_MISC = 0x04000000;
IN_STAT_COMP = 0x05000000;
IN_STAT_ADC0 = 0x06000000;
IN_STAT_ADC1 = 0x07000000;
IN_STAT_MATRIX0 = 0x08000000;
IN_STAT_MATRIX1 = 0x09000000;
ANA_STAT0 = 0x0A000000;
ANA_STAT1 = 0x0B000000;
ANA_STAT2 = 0x0C000000;
ANA_STAT3 = 0x0D000000;
ANA_STAT4 = 0x0E000000;
ANA_STAT5 = 0x0F000000;
ANA_STAT6 = 0x10000000;
ANA_STAT7 = 0x11000000;
ANA_STAT8 = 0x12000000;
ANA_STAT9 = 0x13000000;
ANA_STAT10 = 0x14000000;
ANA_STAT11 = 0x15000000;
ANA_STAT12 = 0x16000000;
CONFIG = 0x1A00040C | 0x00001000 | 0x00000800;
IN_EN = 0x1BFFFFFF;
CS_SELECT = 0x1C0003FF;
WC_CFG0 = 0x1DB6DB6D;
WC_CFG1 = 0x1E16DB6D;
CCP_CFG0 = 0x1F000000;
CCP_CFG1 = 0x20000000;
THRES_COMP = 0x21000000;
INT_EN_COMP1 = 0x22FFFFFF;
INT_EN_COMP2 = 0x23FFFFFF;
INT_EN_CFG_0 = 0x24000004;
INT_EN_CFG_1 = 0x25000000;
INT_EN_CFG_2 = 0x26000000;
INT_EN_CFG_3 = 0x27000000;
INT_EN_CFG_4 = 0x28000000;
THRES_CFG0 = 0x29000000;
THRES_CFG1 = 0x2A016800;
THRES_CFG2 = 0x2B00D247;
THRES_CFG3 = 0x2C045C77;
THRES_CFG4 = 0x2D0CBDA2;
THRESMAP_CFG0 = 0x2E000000;
THRESMAP_CFG1 = 0x2F023000;
THRESMAP_CFG2 = 0x300001F5;
MATRIX = 0x31000000;
MODE = 0x32000000;