Hi team,
The customer is using DP83849IFVS-EVK. The A port can output the data. The led_speed of the A port is turned on all the time.
But he cannot output the data for the B port. When he enable FX-EN,AN0,AN1 and ANEN_B using the default configuration,
the led_speed of the B port is turned off. When he disable FX-EN, the B port cannot be used.
The customer needs to use the B port to output the data. Would you provide some suggestions?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments