Other Parts Discussed in Thread: SN75176A,
Hi,
We used SN75176A in our project for RS485 MODBUS communication. But when we test it on field, due to fail safe resistor presence the number of drivers/units that can be interfaced with the master-node reduced to 3. To increase the number of nodes {32 drivers(including one master} via MODBUS communication up to 1200m, we are looking for an alternative in SN65HVD82DR part.
Can anyone confirm if we use the alternate (P/N:SN65HVD82DR ) our above said requirement can be met or not.
Also please share the fail safe bias resistor value used in SN65HVD82DR for our theoretical calculation.
Regards,
Lakshmy V