This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DS25BR120: DS25BR120 Transmission Characteristics

Prodigy 20 points

Replies: 2

Views: 223

Part Number: DS25BR120

Hello,

I'm looking for someone to identify the transmission characteristics of the  DS25BR120 component. I will be transmitting a signal across a triax cable approximately 50 Ohms at a length of 125 feet. Essentially, I'm, looking to see if this IC is a good fit. The datasheet says that the component is capable of transmitting across metallic cables but does not give any properties of such things.

  • Hi Jarel,

    The DS25BR120 is intended for 100 Ohm cables.  It can transmit into a 50 Ohm cable, but the signal amplitude will be lower than normal.

    The actual transmission distance will depend on several cable variables.  Do you know the cable attenuation per unit length at the desired data rate?

    Regards,

    Lee

  • In reply to Lee Sledjeski:

    Lee,

    Thanks for the update. If that's the case, this may not work. The attenuation is 25 pF per foot. I'll look over this and see what happens. Thanks for you update.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.