Dear TI engineer:
There are 5 problems of DP83TC811S-Q1, please help to answer:
1, If my customer use SGMII interface, need set MAC(2-0) :000
And the 4 level bootstrap as below, does it mean SMGII interface only in Mode 1(RX_P, RX_M)?
Can customer used the resister to set the mode of RX_P and RX_M? Does the MAC interface and Strap mode conflict?
2, How to in sleep mode? Does only need set sleep enabled to “1”? How the "wake" pin set, pull low?
4, What is the max run rate of TRD_P/N?
5, Why MDIO pull-up register is 2.2K to 9K?
Thanks!