I'm using the HVD11 to drive 100ft of wire and associated emi filter capacitance to ground (7Mbps Manchester encoded format). I want to make sure that output waveform does not become too rounded-off due to effects of part's output current limit. Can you tell me if the IOS term "short-circuit output current" of +/-250mA will act as an instantaneous current limit? Need to understand effects this may have on differential rise and fall times when driving a capacitive load.