Hi Guys
Our customers are using our TDP158 as a re-driver for HDMI. Application is Scope.
when we test the Eye Diagram. Input signal is differential signal and the common mode voltage is equal to 0. however We didn't find the output of TDP158 reach the Standard Voltage of HDMI. You can see the out put of TDP158 below. The signal VL is 2.01V and Eye height is 520mV. But we have to make the VL between 2.7V and 2.9V. Right? how to adjust the Eye height by using strap pin or any other solution to adjust it? We don't want to use the I2C to adjust it because of to much software work. The schematic is below. Please check it.
The out put of TDP158:
Schematic:
Any feedback are appreciated. Very urgent issue.
Thanks