This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS30BA101: DS30BA101/DS30EA101 - Balanced Differential 150 ohm

Part Number: DS30BA101
Other Parts Discussed in Thread: DS30EA101, LMH0302, LMH0303

Hello, I would like to use the DS30BA101 and DS30EA101 to transmit and receive 8b/10b encoded data over balanced 150 ohm cable differentially. The cable is about 4 meters long with several matched connectors inline. The data sheets only show 100 ohm differential cable and 75 ohm single ended coax cable applications. Can I set it up for 150 ohm differential termination and adjust Rvo for 800 mV p-p differentially and have equalization and data transmission work properly?

Thanks - philip