Part Number: TPS65986
Hi, all!
I am trying to load the first firmware for tps65986 into spi flash.
Here is the result of the TPS6598x Application Customization Tool
TPS6598x Host Interface Tools gives the same result.
The TPS65986 is powered by VIN_3P3.
LDO_3V3, LDO_1V8A and LDO_1V8D is present. SPI Flash powered from LDO_3V3.
TPS65986 registers are in the following state:
Why PowerSource is Unknown?
Can I, through I2C, read the contents of Flash to a file?
On the oscilloscope I don’t see level changes on flash memory pins when the program is loading.
I ask for help to solve this problem