This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848C: DP83848 Compliance to standards

Part Number: DP83848C

Are there tests performed with UNH on the DP83848 ? Is there a report available ?

Is the DP83848 compliant with :

               Clause 04 - MAC_Test_Suite_v5.3

               Clause 25 - 100BASE-TX PMD_Test_Suite_v3.5

               Clause 24 - 100BASE-X PCS Test Suite

               Clause 31 - Flow Control Test Suite

               Clause 27 - 100BASE-X Repeater Test Suite

               Clause 40- Auto_Crossover_Test_Suite_v2.2

               Clause 28 - Auto-Negotiation State Machine Test Suite

               Clause 28 - Auto-Negotiation Next Page Test Suite

               Clause 28 - Auto-Negotiation Management System Test Suite

               Clause 28 - Auto-Negotiation Management Register Test Suite

               Clause 25 - 100BASE-TX PMD_EEE_Suite_v3.5

  • Hello Herr Eckhardt,

    The DP83848C passes all UNH tests for IEEE clause 14 (10base-t), clause 24(100base-t pcs), clause 25(100base-t pmd), clause 28(AN state machine base page, AN state machine next page), and clause 40 (auto-crossover function). All tests performed by UNH.

    I will share the report offline.

    Best Regards,