Other Parts Discussed in Thread: TIDA-01438
Team,
Can you help me understand if TVS3300 would be able to pass IEC60255-26? i know it can pass IEC61000-4-5 based on TIDA-01438 but the other standard is much more severe.
here are the requirements:
- Line-to Line 1.2/50us (8/20us), 2kV, source impedance 2ohm, coupling resistor 0 ohm
- Line-to earth 1.2/50us (8/20us), 4kV, source impedance 2ohm, coupling resistor 10 ohm
Thanks for looking into this.
Regards,
Dmitry