Other Parts Discussed in Thread: TCA9544A
Hi! First, sorry for my English. I need to make a keyboard with ~280(!) buttons. Is it possible to use 4 x TCA8418 on one i2c bus or is there another solution? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Aleksey,
TCA8418 does not have an address configuration (its slave address is all static). So you cannot connect 4 of them on the same bus together in a normal configuration. It could be possible to do this if you used a switch to select between one of the four TCA8418s at a time. My recomendation would be to use TCA9544A to separate the 4 devices from the I2C line and have an ISR (interrupt service routine) to check which TCA8418 generates an INT (read TCA9544A INT registers).
Thanks,
-Bobby