Hi,
In our design we have used TLK10034 in (XAUI <-->10G Base-KR mode), 4x 10G Base-KR channels are connected to an External Switch (residing on the same PCB). 4x XAUI channels are connected to a XAUI switch. The 4x XAUI channel links are UP. But 10G Base-KR side link is not UP. Auto Negotiation is not completing with value of AN_STATUS register (0x7.0x1) toggling between 0x88 and 0xCD .The Auto Negotiation is not completed on the Link Partner side also.
What might be causing this?