Hi Ti
The datasheet for the pins SS_DN1 and SS_DN2 how are they supposed to interpret?
I intend to put the device into SMBus mode and have both downstream ports support superspeed. Is the SS_DN2 pin an indicator (output) indicating to a microcontroller the status of the port or a control (input) where a microcontroller can set the port type? Datasheet says it is an input but for the SS_DN1 which is the same indicator but for the other port it says it is an input/output. Should not the SS_DN1/2 pins have the same direction?
I interpret that I need to have low level on SS_DN2 on reset to set device in SMBus mode and after reset set SS_DN2 to high level to have superspeed support on downstream port 2.
Same for SS_DN1 to have it low on reset to set device PWRCTL active high and after reset set SS_DN1 to to high level to have superspeed support on downstream port 1.
Can you please clarify?
Br
Imre