This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS0500: why choose TVS0500 over standard SMC TVS diode

Part Number: TVS0500

Dear *,

i have some questions regarding TVS protection

1) When do we have to chose or look at 8/20 waveform and when 10/1000 waveform, how do i know if i need 8/20 protection device or 10/1000 protection device?

2) Why do i choose TVS0500 over traditional TVS diode, what are the benefits?

3) is the steeper i/V of TVS0500 regarding to traditional TVS better and why?

4) What does mean this in ds?

a)

Robust Surge Protection: – IEC61000-4-5 (8/20 µs): 43 A – IEC61643-321 (10/1000 µs): 22 A

b)

Integrated Level 4 IEC 61000-4-2 ESD Protection

Best Regards,

D.