I/O on this device sometimes powers up into a low-output state. I have 10K pullups on all of the Pxx pins. Not all devices show the problem. Currently 2 out of 11 units show the issue.
On one of the units ports P10 and P12 fail low on power up maybe 2% of the time. The other unit usually has only P10 fail. The same 10K pullup (driving a high-impedance input) is used on all GPO pins.
Software cannot be a workaround for this design since critical I/O is being set by the '1' default output.
The device is properly bypassed and +3.3V VCC rail is clean.