This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042HG-Q1: Power supply solution

Part Number: TCAN1042HG-Q1
Other Parts Discussed in Thread: TCAN4550

Hello

As I see, TCAN1042x series did not integrated power supply, do you have below CAN solutions: Output 5V voltage with en/disable control,capable >250mA, support CAN FD,

  • Fandy,

    At the moment, the only CAN device with a voltage output integrated that TI has available is the TCAN4550. This device is a CAN controller and transceiver integrated as well though, not just a transceiver with an integrated power supply.

    Can you explain the application in a little more detail?

    Regards,
  • Hi Eric

    Did Ti have similar solution with NXP's CAN SBC, Like TJA1075/6

  • Fandy,

    I wasn't able to find the TJA1075/6 on the internet, but I was able to find the UJA1075. We don't have anything released at the moment that can be a direct replacement of this device, the closest would be the TCAN4550, but even this solution would not be a suitable replacement in most cases. This would require multiple devices from TI in one solution, we don't currently offer anything integrated with all the features of the UJA1075.

    Regards,