Hi team,
I have a question regarding a SN65HVD233. I’m trying to determine the minimum load resistance this device is capable of driving. All I can find clearly stated in the datasheet is 60ohm+/-1% for various parameters, which I presume may be a test condition and not an operating range.
That said, I’m calculating the minimum load resistance based on drive capability. Is it correct to use the value shown in Table 8.3 (50mA) in combination with minimum Differential Output Voltage (1.5V)?
1.5V / 50mA = 30ohm
Thanks for any assistance.
Brian