Other Parts Discussed in Thread: TCAN332, SN65HVD1050
Hi,team.
I want to operate TCAN332EVM with split termination and nomal mode.
i have 3 question.
①How should I set JMP 6?
②I think , I can operate split temination mode with only implement 60Ω in R7 and R15, 4.7nF in C4 .
is this right?
2.1.11 in User's Guide say [If the device and application support split termination the JMP6...].
Are there conditions other than R7, R15, C4 to operate with split termination?
③what does mean Table 5. in User's guide , Device pin No.5 ?
In datasheet of TCAN 33x, pin No.5 has NC/SHDN/FAULT function.
What is Vref/SPLIT?
If I want to operate split termination mode , should i think about Vref/SPLIT?