This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS1800: Can it do Protection Against ±0.5Kv, 2 Ω IEC61000-4-5 ?

Part Number: TVS1800

Hi 

Can TVS1800 do Protection Against ±0.5Kv, 2 Ω IEC61000-4-5 ?