Other Parts Discussed in Thread: HD3SS460
hi
i`m deloping usb hub
Could you please Program request for EEPROM connection for register control of tusb 8020b
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I created a circuit with reference to TUSB8020BPHPEVM Schematic,
but it does not work. Ask if you need to put binaries in eeprom or just usb hub operation through dip sw control.
sllu196.pdfAlso ask the eeprom programmer file
Hi Kim,
TUSB8020B should not need to be programmed when powered up into I2C mode. When you say your board does not work could you describe the failing condition?
I would start with using the default state of TUSB8020B first to debug this issue and then customize your implementation with TUSB8020B register values. Could you post your schematic for review?
hi
How to enter i2c mode tusb8020b ?
As you suggest i cheked the status of the switch.
SW1_1 (on): FULLPWRMGMTZ_SMBA1_SS Switch
SW1_2 (off): PWRCTL_POL_SS_DN1 Switch
SW1_3 (off): SMBUSz_SS_DN2 Switch.
SW1_4 (on): GANGED_SMBA2_HS Switch
SW1_5 (off): SCL_SMBCLK Switch
SW1_6 (off): SDA_SMBDAT Switch
SW1_7 (off): PWRCTL1_BATEN1 Switch.
SW1_8 (off): PWRCTL2_BATEN2 Switch