This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS280DF810: What's the max value of VIDmax? what's the DC voltage stress of the internal cap?

Part Number: DS280DF810

Hi team,

we want to check below two items.

1. What's the max value of VIDmax?

2. what's the DC voltage stress of the internal cap?

Thanks.

  • Hi Frank,

    1). Actually max VID is 1225mV. This is not called for in the data sheet because if we have this listed it means - per TI policy - every device has to be tested against this parameter in production and this is not what is done at the moment.

    2). Please note absolute maximum ratings. . Maximum IO DC supply is 2.75V. This means DC voltage on analog signals should be below 2.75V.

    Regards,,nasser