Other Parts Discussed in Thread: ASH
Hi,
I want to use this IC for the HDMI purpose in the pin strapping mode.
I have following doubts:-
1. SoC side my voltage for DDC signals is 1.05V. I am using the LT which convert 1.05V to 3.3V.
Can I use this topology
SoC(1.05V) <--> LT(1.05 to 3.3V) <--> TDP158 <--> HDMI connector.
The doubt came as the datasheet suggest to use below topology ( datasheet Figure 46)
SoC(1.05V) <--> LT(1.05C to 5V) <--> HDMI connector.
2. I want to understand the use of SWAP pin.I am not clear as it mention in the datasheet.
3. I will using this IC in pin strapping mode. I want to understand the pin fumctionality of EQ1/A0 and EQ1/A1 pins
Thanks
Ash