This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4420: can TCAN1042DEVM be used for TCAN4420?

Part Number: TCAN4420
Other Parts Discussed in Thread: TCAN1042DEVM,

Team,

can TCAN1042DEVM be used for TCAN4420?

http://www.ti.com/tool/tcan1042devm

Thanks,

A.

  • Hello,

    Yes, these devices have compatible pinouts and so the TCAN1042 EVM can be used to evaluate TCAN4420. The only difference would be the meaning of pin 8 (which is a logic input that can be pulled high or low on the EVM).

    Max