Dear All,
My Japanese customer has a question about TUSB2036. The question is below:
I need to connect a low-speed USB device to a USB host that supports only full-speed. Is this possible by inserting TUSB2036 as a HUB between host and device?
The USB host we are considering using is the USB host controller with built-in Renesas RX63N MCU. The note2 in 1208 page of user's manual (hardware) of RX63N states that "The USB controller does not support communications with a low-speed device." I consider that it corresponds to Full-Speed only.
Although this is the “USB Bus Reset” only, will it affect the normal USB date transfer?
RX63N Group, RX631 Group User's Manual-Hardware-en.pdf
Pls help me
BR
Tom.Liu