This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3USB31: Layout check

Part Number: TS3USB31

Hi Sirs,

Sorry to bother you.

Generally,the incoming and outgoing lines should be parallel? How is 2 in 3 out, 5 in 6 out

Is this going to be smooth?

Look at the block diagram & Package, HSD1+ is connected with D+, HSD1- is connected with D-

This way, the line that feels coming out has no way to always be differential.

Could you check the actual layout file can share? Like the public board?

However, it seems that it is impossible to maintain the space of the 90 ohm differential trace.