This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 155
Part Number: TS3USB3000
I have question
I have just find KO = 1.75 mm in 21p. Please see the below.
But I found below in 25p.
So I want to make sure what point is different between p21 and p25?
And I am afraid that if K0 is 1.75mm, The hole is large relative to the dimensions of the device itself and I an wondering it will rotate when you shake the box .
Please give your comment,
Best regard
let me find and update ASAP.
In reply to Brian Zhou:
0.75 is correct, we ill update datasheet soon.
Hi Zhou
customer also ask me some question.
The previous data sheet had 2 types of specifications (1 pin position of TS3USB3000RSER is Q1 or Q3).This time only one type (1 pin position of TS3USB3000RSER is Q1).I would like to make sure One more kind (the 1 pin position of TS3USB3000RSER is Q3) could be abolished?Also, if you order in the near future, will the TS3USB3000RSER 1 pin position receive a taping product with Q1?It will be helpful if you can confirm.
Thank you for your kind help
Yuki Saito
In reply to Yuki Saito:
yes, only Q1 right now.