Hi,
- When VCC=0V, is the output pin (ROUT1, ROUT2) state high-impedance or connected to GND?
- When would WSON be available?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Thanks.
Hello,
I am looking into this and will get back to you on the state of the outputs (ROUTx) when the device is not powered. I think they will be high impedance, but trying to confirm.
Regarding the SON package, samples are available now, and production is expected in 4Q.
Regards,
Yaser
Hi,
There are ESD diodes to VDD and GND on the output pins. This will make a low impedance path to GND if any signal large enough to turn on the diode to GND. For signal amplitudes between -0.3 and +0.3V I would expect a relatively high impedance.
Regards,
Lee