Hi,
Customer is asking whether SN75DP130 is recommended for cable length up to 20m. Protocol is DP1.2, 4k.
Would you recommend other ICs?
Thanks & BR,
KF
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
KF
Do you have a block diagram? What is the insertion loss of the cable?
For DisplayPort, TI has two solutions:
DP139 is a limited re-driver which the transmitter provides its own SWING and Pre-emphasis, different from the DP source SWING and Pre-emphasis.
DP142 is a linear re-driver which the transmitter does not have its own SWING and Pre-emphasis.
Either one of them can be used depends on the system application requirement.
They can order a EVM and use it to evaluate the cable.
Thanks
David