Dear TI Team,
In the sleep mode, we will ask for the leakage current value when the switch input is ON.
In case of Sleep mode in Switch On state, Leakage current is high and it needs confirmation.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Team,
In the sleep mode, we will ask for the leakage current value when the switch input is ON.
In case of Sleep mode in Switch On state, Leakage current is high and it needs confirmation.
Thanks.
Hi, Youngsu,
When the TIC10024-Q1 is put into the sleep mode (polling mode) and when the input is not getting sampled, the leakage current for each input is the same as if the channel is disabled and it's spec'ed in the datasheet as below. The leakage current is specified regardless of whether the external switch input is ON of OFF as it is only a function of the voltage on the VINX pin and the temperature.
Regards,
David
Dear David,
Thank you for answer.
We encounter the following phenomenon.
1. INx : S/W ON (GND)
2. Idle state
3. 60 ~ 80uA current per channel is confirmed (current increases as channel increases)
In the above conditions, it is necessary to confirm whether or not the setting is wrong.
Can you confirm the settings to reduce the current under the above condition?
Thanks.
Hi, Youngsu,
That seems a little bit too high. Can you confirm whether:
Thanks,
David
Yonungsu,
We haven't heard from you in a while so we will assume you resolved your issue. I will close this thread but you may reply here to reopen it or create a new thread if you have additional questions.
Thank you,
Adam