This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TUSB8041-Q1: Is AC coupling cap at USB_SSTXP_UP and USB_SSTXM_UP line needed when intra-board connection?

Intellectual 2165 points

Replies: 1

Views: 76

Part Number: TUSB8041-Q1

hello, the datasheet says 100nF coupling cap is needed for SSTXP and SSTXM. is this still needed when connection is done in the same board?

ito 

  • Hi,

    This capacitance is still need in this case. USB spec requires AC coupling capacitance on the super-speed transmitter so this is also required on the USB Host SSTX even though connection is on the same board. 

    Best, 

    Malik

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.